AS-i and IO-Link – a good connection.

AS-i and IO-Link – a good connection.

AS-i module with 2 IO-Link ports.

  • Easy parameter setting of the IO-Link devices.
  • Extended diagnosis for IO-Link devices.
  • Loss-free data transmission.
  • IO-Link master for sensors and actuators.
  • Communication down to the sensor.
AS-i and IO-Link
IO-Link is the intelligent connection between the device (sensor or actuator) on one side and PLC or field module on the other side. With the IO-Link AS-i module you combine the advantages of the AS-i wiring system with the standardised IO-Link communication. Using the simple AS-i connection technology you establish the data connection and energy supply for IO-Link devices - sensors and actuators. The sensor settings are saved in the AS-i module and can be transferred to a new sensor, if necessary.

AC5225 - Active ClassicLine module, 2 IO-Link ports, For the connection of IO-Link sensors and actuators, binary sensors and binary actuators, Addressing socket, Three orientations of the flat cable are possible, IP 67, Ambient temperature -25...70 °C

Current bulletin