Positiesensoren en objectherkenning Processensoren en diagnosesystemen Bussysteem AS-Interface Besturingssystemen Identificatiesystemen

 
Electronic pressure switch PNI with analogue input.
 
 

 
Functionality
The ifm pressure sensor offers a new means of signal evaluation.The two freely configurable switching outputs can be continuously and automatically adjusted using an analogue input signal (4-20 mA / 0-10 V). The display indicates either the input pressure, the output pressure or the differential pressure.

differential pressure switchApplication example
Variable pressures are used in the hydraulic clamping systems for machine tools: It is a significant advantage if the switch point can be adjusted electronically in response to changes in the valve position. Clamping pressure is to remain within a variable acceptable range (window). If the pressure is outside the preset window the switched output is de-energised. Special feature: The acceptable range is varied using an external analogue signal.

Differential pressure switch
By evaluating the analogue signal of an external pressure transmitter the sensor switches if the set differential pressure is too high or too low. Applications include monitoring of filters or balancing liquids in tanks. Since the reference measurement is an electrical signal rather than a physical variable it is easy to monitor a differential pressure between remote locations.

performance feature
  • Evaluation of external voltage/current values.

  • Continuous comparison of set/actual values within the sensor.

  • Integrated task specific functions..

  • Monitoring of differential pressure by processing a pressure transmitter signal.

  • 4-digit LED display,pressure indication in bar,psi,and MPa.

 PNI021 - pressure sensor measuring range 250 bar
 PNI022 - pressure sensor measuring range 100 bar
 PNI024 - pressure sensor measuring range 10 bar


Further information:
 download of pressure sensor bulletin (PDF-File 525kB)