ifm electronic - Pressure sensors
- Transmitters or sensors with integrated control monitor.
- Overload protection and high long-term stability due to a ceramic measuring cell.
- Measuring range up to 600 bar.
- Optional fittings for variable process connection.
- EPS interface for external programming.
Product search - ifm pressure sensors
ifm Product line
Contact
Introduction
The ifm pressure sensors have been developed for monitoring system pressure in hydraulic and pneumatic applications. Today we cannot imagine the food industry or hygienic applications without pressure sensors. ifm offers a variety of different types for different industrial applications. All units have one thing in common: They have a one-piece housing and need no moving parts such as pistons or springs. The result: The sensor are extremely robust against mechanical influence and work completely without wear and tear and fatigue. The sensor has a ceramic measuring cell. The advantage of this material is that it is resistant to corrosion and gives long-term stability. In the long run this guarantees a continuous accuracy of the measured values. ifm sensors are also resistant to dynamic pressure peaks and have a high overload resistance. It is of special importance that they are resistant to pressure peaks which usually arise on fast closing valves. Depending on the mounting position pressure peaks as well as vacuum peaks can alternate quickly. Even in these critical situations ifm sensors are resistant. The flush sealing system of the ceramic measuring cell when mounted in the stainless steel housing allows optimum cleaning of the sensor – an absolute must for the use in the food industry or in hygienic applications.
ifm electronic
ifm electronic gmbh is one of the leading manufacturers of automation technology world-wide. More than 3,000 employees in more than 70 countries develop solutions for 80,000 customers in the manufacturing industries. By optimising technical processes in the automotive, chemical and cosmetics industries or in environmental technology and automation of buildings ifm electronic has consistently set new standards and thus ensures tomorrow's production processes.
The family-run company with headquarters in Essen started with the invention of inductive proximity sensors in 1969. The German production in Tettnang on Lake Constance has ensured brand quality right from the start. Today "efector" stands for position and fluid sensors, object recognition, diagnostic and identification systems. The brand "ecomat" is synonymous with networking and control systems. In 2007 ifm made a turnover of more than € 410 million with above-average product quality, exceptional innovations and consistent close contact to the customer.