ifm electronic - Incremental encoders

  • High switching frequencies.
  • Robust designs.
  • Programmable encoders.
  • Special version with integrated Profibus interface.
  • Hollow shaft encoders for drives with high acceleration.

Product search ifm encoders
ifm Product line
Contact
Introduction
In many manufacturing and production processes they are indispensable as reliable transducers to ensure precise positioning. They convert rotary movement into digital signals. Linear measurement is also possible in conjunction with rack and pinion or measuring wheels. Encoders use the wear-free photoelectric detection. A pulse disc firmly attached to the shaft ensures this detection.

Incremental encoders generate a precisely defined number of pulses per revolution. They are a measure of the angular or linear distance moved. The coded disc is divided into separate segments which are alternately transparent or opaque. An LED emits a parallel-orientated light beam which illuminates all segments of the coded disc. Photo elements receive the modulated light and convert it into two sinusoidal signals. Digitalisation electronics amplify the signals and shape them into square-wave pulse trains which are generated via the line driver in the output. The phase difference between signal A and B, which are phase-shifted by 90 degrees, allows evaluation of the direction of rotation.

ifm electronic
ifm electronic gmbh is one of the leading manufacturers of automation technology world-wide. More than 3,000 employees in more than 70 countries develop solutions for 80,000 customers in the manufacturing industries. By optimising technical processes in the automotive, chemical and cosmetics industries or in environmental technology and automation of buildings ifm electronic has consistently set new standards and thus ensures tomorrow's production processes.

The family-run company with headquarters in Essen started with the invention of inductive proximity sensors in 1969. The German production in Tettnang on Lake Constance has ensured brand quality right from the start. Today "efector" stands for position and fluid sensors, object recognition, diagnostic and identification systems. The brand "ecomat" is synonymous with networking and control systems. In 2007 ifm made a turnover of more than € 410 million with above-average product quality, exceptional innovations and consistent close contact to the customer.