Photoelectric sensor monitors cheese production
Requirement
In cheese presses the remaining whey of the curd in a cheese mould is forced out by mechanical pressure. After filling the press numerous compressed air cylinders apply the required pressure.
Implementation
ifm through-beam sensors of the OG wetline series monitor the correct function of the compressed air cylinders in each string of the press.
Customer benefits
If after pressing a compressed air cylinder does not return to its initial position, emptying the cheese press can lead to damage and downtime. This can be avoided by detecting the individual cylinders.
In cheese presses the remaining whey of the curd in a cheese mould is forced out by mechanical pressure. After filling the press numerous compressed air cylinders apply the required pressure.
Implementation
ifm through-beam sensors of the OG wetline series monitor the correct function of the compressed air cylinders in each string of the press.
Customer benefits
If after pressing a compressed air cylinder does not return to its initial position, emptying the cheese press can lead to damage and downtime. This can be avoided by detecting the individual cylinders.
Products used in this application
More applications in this product group
- Continuous bearing monitoring on a separator
- efector metris compressed air meter monitors cheese production
- efector pmd optical distance sensor monitors ice-cream production
- Level detection on a tank
- Photoelectric sensor monitors cheese production
- Position feedback on pneumatic cylinders
- Pressure monitoring in homogenisers
- Run-dry protection on a pump
- Temperature monitoring on a heat exchanger
- Vibration diagnosis on a homogeniser