Object recognition "bearing present" in gearbox assembly
Requirement
In the production of gear shafts a sensor is used to check if a needle bearing has been installed, if it is the correct bearing and if the installation has been carried out correctly.
Implementation
The efector dualis contour sensor (order no. O2D215) is used for this task together with a background illumination unit (order no. O2D905). The contour comparison, by means of a backlight, ensures that the shaft meets the quality requirements of the customer.
Customer benefits
The assembly process is quickly, conveniently and precisely monitored. Another visual inspection is not necessary. The application could be solved at a low cost using the efector dualis contour sensor.
In the production of gear shafts a sensor is used to check if a needle bearing has been installed, if it is the correct bearing and if the installation has been carried out correctly.
Implementation
The efector dualis contour sensor (order no. O2D215) is used for this task together with a background illumination unit (order no. O2D905). The contour comparison, by means of a backlight, ensures that the shaft meets the quality requirements of the customer.
Customer benefits
The assembly process is quickly, conveniently and precisely monitored. Another visual inspection is not necessary. The application could be solved at a low cost using the efector dualis contour sensor.
Products used in this application
More applications in this product group
- Level monitoring in a parts washer
- Level monitoring in a swarf hopper
- Level monitoring of oil in a hydraulic power pack
- Object recognition "bearing present" in gearbox assembly
- Position monitoring of brake disks
- Position verification on a roller conveyor
- Pressure control of hydraulic power packs
- Pressure monitoring in a parts washer
- Temperature monitoring of hydraulic oil