Position sensors and object recognition Fluid sensors and diagnostic systems
2-wire pressure sensor, parameter setting via IO-Link. On-site control monitor for flow sensors. Temperature plug type TP: modular transmitter Compressed air meter with display and totalizer function. Diagnostic electronics with fast reaction time New additions to the temperature probe range. New Pt100 sensors for industrial applications Combined oil moisture and temperature sensor. Interface for automation technology: the OPC server software Pressure sensor for robotics and handling Reliable overflow protection of liquids. Compressed air consumption and leakage monitor Continuous vibration monitoring Electronic manometer PG, with alternative process connection Hydrostatic level measurement in hazardous areas Pt100 / Pt1000 bolt-on and screw-in sensors Hygienic point level sensor with complementary output Archive
Bus system AS-Interface Control systems Identification systems

 
Standard USB interface for parameter setting of sensors.
 
 

 
For parameter setting of sensors before or during set-up.
  • Quick and easy to mount.
  • Supports the parameter setting of IO-Link and EPS sensors.
  • In combination with FDT manufacturerindependent exchange of data.
  • Device configuration, documentation and diagnostics for the entire plant.
  • No additional sensor supply required.

USB interface for parameter setting of sensors
The USB interface has long been established as standard interface on common PCs and notebooks and replaced the RS-232 interface common in the past. ifm allows for this development and provides an USB interface (USB 2.0) enabling direct parameter setting of IO-Link and EPS sensors via the USB interface of a computer. To do so, the sensor to be parameterised does not have to be supplied via an additional power supply. The unit is directly supplied from the PC. In combination with the ifm Container, which is provided free of charge on CD, parameter setting and documentation are a child’s play.

Use in combination with the FDT technology
The USB interface can be used in combination with the supplied ifm FDT Container. The FDT technology standardises the communication interface between field devices and the system environment. The special feature of this technology is that it is independent of the communication protocol used and the software environment. Moreover, the user is independent of the selected unit and control system used. In brief: With FDT it is possible to address any unit via any system using any protocol – now also via the standardised USB interface.

System requirements:
• Windows 2000 / XP / Vista
• free USB 2.0 port
• 1 MB free memory space on hard disk
• installed FDT or EPS software

E30396 - USB-IO-Link / EPS interface


Further information: Bulletin (PDF file 483 kB).