Sensores de posicionamento e detecção de objetos Sensores de fluído e Sistemas de Diagnósticos Rede AS-Interface Sistemas de Controle Sistemas de Identificação Sistemas de identificação

 
New variants of the innovative PK pressure switch generation.
 
 

 
The ingenious solution with new output function.
  • 2 separate switching outputs with fixed hysteresis (2 %).
  • Easy switch point setting using two setting rings for optimum readability.
  • Stainless steel measuring cell, e.g. for freons in refrigerating technology.
  • Mechanical locking prevents inadvertent switch point manipulation.
  • High bursting pressure range for gases and liquids.

The new solution
The compact ifm PK pressure switch series is the first electronic pressure switch to feature a successful combination of easy setting and high long-term stability.
This pressure switch is distinguished by a high pressure peak resistance and excellent resistance to aggressive media. Units with two separate switching outputs and a fixed hysteresis have now been added to this series. The fixed reset point is 2 % of the freely adjustable set point.
As a result of the consistent further development of this innovative series the sensors can be used in more applications. This gives the user more flexibility in almost all industrial and mobile applications.

Award-winning
ifm pressure switch of the series PK won 'Leonards Trophy 2004' in the category 'Best components and automatism periphery'. This prize is awarded on the exhibition Automation Optimation Europe in Paris.
in Paris vergeben. Further Information: ifm press release (PDF-File 8 kB).

The easy operating concept
The ease of handling is fascinating: Due to the radial setting rings with a unit scale in bar and psi for optimum readability every user can adjust the set point and reset point quickly and precisely even without pressure being applied. Due to the possible mechanical locking inadvertent manipulation is excluded. A protective cap that is available as an accessory protects against manipulation.

Versatility
The robust pressure switch can be used in nearly all industrial and mobile applications. Not only standard hydraulic and pneumatic applications can be implemented, but also gas pressures up to 400 bar or applications in air conditioning and refrigerating technology. The maximum robustness of the stainless steel measuring cell ensures high long-term stability and wear-free operation over millions of pressure cycles.


Leonards Trophäe 2004

Stainless steel measuring cell welded without seal · Process connection G 1/4 male · Protection rating IP 67

(PNP) · output 2
 PK7520 - Measuring range relative pressure 0...400 bar
 PK7521 - Measuring range relative pressure 0...250 bar
 PK7522 - Measuring range relative pressure 0...100 bar
 PK7524 - Measuring range relative pressure 0...10 bar

output 2 · 2 x PNP complementary
 PK6520 - Measuring range relative pressure 0...400 bar
 PK6521 - Measuring range relative pressure 0...250 bar
 PK6522 - Measuring range relative pressure 0...100 bar
 PK6524 - Measuring range relative pressure 0...10 bar

  Virtual product presentation (flash animation)
  File with integrated flash player – EXE file 750 Kbytes


 
3D Panorama (flash animation)
Flashanimation PK6520

Remarks:
Please ensure that the current flash plugin (version 5 and above) is installed in your browser. If not, this plugin can be downloaded free of charge from Macromedia. Interested persons who do not want to install the plugin can download a directly executable file (EXE file) with integrated flash player from us.

Operation is normally done using the mouse. Please finish the animation by closing the separate browser window.